Honeywell Security UK

CONTACT & SUPPORT  |  WORLDWIDE        

 Search
Government

The town of Plaisir entrusts its protection to the Galaxy Dimension security solution
Plaisir is a vibrant town, located 20 miles from Paris in the Ile-de-France region of France. Plaisir has the seventh largest population in the Yvelines area, with over 50% of its inhabitants in work and 30% under the age of 19.
Transforming urban living through security
Sunderland Housing Group (SHG) is a not for profit organisation that manages tenanted housing of over 36,000 homes, among which are 23 tower blocks - situated across Sunderland City. Originally built in the 60s, the towers had become rundown as a result of on-going vandalism, tenants being harassed and under occupancy.
Nottingham City Homes
Nottingham City Homes, previously part of Nottingham City Council, and now a limited company, is responsible for over 30,000 tenanted properties in and around the City of Nottingham.