The Client:
Located in Northern Ireland, The OUTLET is the area’s newest designer outlet shopping centre.
With over 60 shops including numerous designer fashion brands and national
retailers as well as a wide range of restaurants and cafes, it attracts shoppers from all
over Ireland.
For this leading European outlet destination containing big-brand retailers with high value
merchandise on sale, the management company required a comprehensive CCTV
management solution that would protect its visitors, premises and ultimately help to
reduce shrinkage from the retail units.
The Situation:
As a newly-built shopping centre, a state-of-the-art digital CCTV solution was required to
provide video surveillance to all the areas outside of the shops themselves. This included
the main 0.5km long public walkway, the 1500-space car park and the service yard areas
behind the shops. Such a requirement would help attract some of the biggest names in
retail to occupy the retail units.
Whilst each retailer has its own security
system and staff, The OUTLET required its
own security team to work in partnership
with the retailers to offer a comprehensive
security solution for the entire centre. This
would help to detect and deter incidents on
site and ultimately contribute to reducing
shrinkage for each retailer.
The system specification included
innovative products with industry-leading
features and demanded the highest quality.
It was imperative that CCTV images of
evidential quality could be captured and
recorded to ensure a high conviction rate
when needed.
The recording solution needed to be easy to
use with real-time recording so that an
immediate response to any incidents could
be implemented.
Finally, it was important that the design of
the CCTV domes complemented the
shopping centre’s contemporary design
providing effective and aesthetic monitoring.
To find the security solution that would suit
its needs, The OUTLET undertook a tender
process to select a preferred supplier.
The Solution:
The OUTLET chose the Fire & Security
integrator Building Protection Systems
Northern Ireland Ltd. (BPS) to carry out the
project. BPS proposed the installation of a
system from Honeywell Security, offering
premier quality surveillance using leading
technologies from a single source.
Full colour CCTV surveillance is provided
during the day, with an automatic
changeover to mono at night when light
levels are lower ensuring that the quality
of the image is maintained. To achieve this
a system of 34 high-powered cameras
covering the walkways, car park and
service yard areas was installed using
wall- and pole-mount microspheres from
the Honeywell Orbiter range. The easy to
set-up presets assist in the establishment
of a number of programmable camera
‘tours’ encompassing pan, tilt and zoom
sweeps of key areas of the shopping
centre. Perfect picture quality is achieved by advanced auto focus control to ensure
that, no matter what the zoom position the
picture is in the sharpest-possible focus.
Covering service vehicle delivery areas and
the car park, Orbiter microspheres have
been deployed to maintain a watchful eye
in these areas too. The high power zoom
capability of the domes positioned on poles
ensure that the vicinity around the centre
can also be seen clearly to help prevent
security breaches from occurring before
any suspected criminals reach the shops.
If there is an incident, the images can be
checked within seconds to get information
and evidence to pass on to the police.
These microspheres are connected via a
Videoblox 64/8 matrix with images
recorded and stored on four HRHD 320GB
Digital Video Recorders (DVR). The DVR
has a built in multiplexer that can record up
to 16 cameras at the same time. The
HRHD DVR is easy to operate and offers
real-time recording.
This Honeywell DVR was recommended
because of its high quality performance,
multi functionality and because it makes it
easy to retrieve CCTV images via the
in-built CD writer.
Additionally, a new, sophisticated security
control room operating 24/7 was
established. Here all the captured images
are recorded and viewed live via five 19 inch
Honeywell TFT colour LCD monitors.
Cameras and scenes are easily controlled
by the ergonomic Videoblox programmable
keyboard controller.
This control room also houses the site’s
dedicated security team. Thanks to the high
power zoom on the cameras that provides
crystal-clear detail, the security team can
easily communicate with security personnel
located outside of the control room to alert
them to react to and prevent security
breaches.
The ongoing relationship between BPS and
Honeywell means that The OUTLET is able
to benefit from the Honeywell ‘Advance
Replacement’ programme, ensuring that
the system is always fully operational.
“The Honeywell
security system
installed enables us
to monitor all public
areas of the shopping
centre effectively. It is
very easy to use and
contributes enormously
to offering our
customers a safe and
enjoyable shopping
experience.”
Euan Forbes,
Centre Manager for The OUTLET
The Benefits:
Using a solution from Honeywell, The
OUTLET now has a state-of-the-art
security system helping to deter theft and
to protect its customers, premises and car
park.
The security system installed not only acts
as a deterrent but, when needed to supply
evidence in order to catch shoplifters, it
can provide high quality images with
minimum delay.
The Honeywell HRHD 16 DVRs installed
ensure that all recorded content can be
retrieved easily and events searched
speedily. The CCTV images can quickly
and easily be transferred on to a CD and
provided to the police in relation to a
specific incident time and date.
The result is that security breaches are
deterred and the in-store security teams
are confident that any criminal activity can
continue to be recorded outside of their
store; resulting in reduced crime
and a safer shopping experience for
customers.
Euan Forbes, Centre Manager for The
OUTLET comments, “The Honeywell
security system installed enables us to
monitor all public areas of the shopping
centre effectively. It is very easy to use and
contributes enormously to offering our
customers a safe and enjoyable shopping
experience.”
Partner of Choice:
BPS was founded in 1981 and is a
supplier of services in design, installation
and maintenance of systems including
Fire Alarms, Intruder Alarms, CCTV,
Access Control and Baby Tagging
Systems, connected to integrated Alarm
Management Supervision Systems.
The Products:
- 34 x Orbiter Domes: mixture of wall,
pole and soffit mount
- 4 x Digital Video Recorders Duplex
320GB: HRHD16C320X
- 5 x LCD Monitors: HMLCD19X
- 1 x VideoBlox 64/8 Matrix: VBLKIT-6408
- 1 x Systems Keyboard: HVBPCKV
Comprehensive Security for Retail Outlet (pdf) |