Sunderland Housing Group (SHG) is a not for profit organisation that manages tenanted housing of over 36,000 homes, among which are 23 tower blocks - situated across Sunderland City. Originally built in the 60s, the towers had become rundown as a result of on-going vandalism, tenants being harassed and under occupancy.
If you have installed a Honeywell Security system and would like Honeywell to create a case study to promote the application please, click here to send us more details. Please note that we will need the end user’s permission to publish prior to commencement of the case study and prior to publication.