The Client Costing £60 million and measuring 85 metres (265 ft) in
height, Obel dominates the Belfast skyline. It has overtaken the current tallest
skyscraper in Ireland which is Windsor House (80m) and is also in Belfast. Obel
was developed by the Karl Group and is located on Donegal Quay on the river
Lagan beside the Lagan Weir. The development consists of 282 luxury apartments
and this ultra modern construction has two underground car parks and commercial
and retail space in development.
The Situation Blackbourne
Integrated M&E is the electrical and mechanical contractor responsible for
all aspects of management of the buildings and facilities at Obel.
Building Protection Systems (BPS) based in Belfast is the security
installer for the project and specialises in the specification, installation and
maintenance of security, video, access, fire and intrusion systems.
Karl Group, the company that owns Obel, has an obligation to provide safe and
secure parking for residents. As an exclusive address in the heart of Belfast,
residents expect their cars to be monitored and for thieves or vandals to be
deterred from any illegal activity. Equally residents expect the entrance and
central lobby area of the tower to be monitored closely to prevent intruders and
unwanted guests from entering the building.
“We are pleased that we were chosen as specialist sub-contractor for the
supply & installation of security and fire systems for this prestigious
project”, said Clive Kinnear, Senior Manager Security Systems, BPS Northern
Ireland. “We have worked closely with Blackbourne Integrated M&E to ensure
that our systems were installed on time for the completion of the
building.”
For the Obel project, Blackbourne required a cost effective CCTV solution
with the capacity to record and store surveillance footage to provide 24/7 video
monitoring of the underground car parks and lobby area of the building. Part of
the requirement was for the cameras to be vandal resistant and able to withstand
the damp environment of the underground car park as it is very close to the
river Lagan.
BPS turned to Honeywell to deliver the right product mix for this project. As
a market leader in video surveillance, CCTV and digital video recording
solutions, Honeywell provided the right equipment to meet the clients’
requirements.
The Solution With the
requirements clearly defined, Honeywell was able to provide the cost effective
solution specified by BPS and Blackbourne Integrated M&E.
The two underground car parks have been fitted with 21 Honeywell HD4 vandal
resistant colour mini domes for the following reasons:
- Resistant to attack whilst having an environmentally suitable housing.
- Delivers high quality pictures and resolution.
- Cameras are able to withstand the rigors of the car park environment –
damp, cold, moist and low light conditions.
The HD4 provides a camera and lens as a single, vandal resistant, compact
unit that is easy to install. The rugged scratch resistant 3.5 mm thick
polycarbonate construction can withstand heavy external impacts. In addition,
the housing incorporates a new vent that prevents any condensation from forming
inside the housing. This innovative camera, with waterproof properties, meets
IP66 standards for critical outdoor installations.
Three Honeywell HD3 Series colour mini domes are deployed in the lobby area
of the building to monitor people entering the building and lift usage.
The HD3 Series was used for the following reasons:
- Captures clear, crisp video and improves recorded video quality when used
with a digital recorder.
- Tamper resistant housing protects the camera and cabling.
- Discreet housing.
The HD3 is a camera and lens unit integrated as a one-piece, tamper proof and
compact unit that can be surface or flush mounted for fast and easy
installation. It is attractive and unobtrusive yet provides a crime-deterring
presence around-the-clock with its excellent low light imaging protection.
Two Honeywell 16 Channel 1Tb HRDPX Performance Digital Video Recorders (DVRs)
have been installed to record and store the video footage from the domes in the
car park and the lobby. They are monitored onsite by a dedicated operator. Two
Honeywell HMLCD 19x LX monitors have been installed to view the stream of
footage collected from the DVRs.
The highly cost effective HRDPX16 Performance Series DVR offers a high image
per second (IPS) recording rate combined with a feature set comparable to many
high-end embedded DVRs.
The HRDPX16 supports continuous, event and combined continuous/event
recording and is configurable per channel. Upon detection of motion, the HRDPX
can automatically boost the images per second recording rate to capture
additional details of the scene. This is a vital feature of the DVR in aiding
the production of video evidence. Once video evidence is located on the HRDPX16,
the user can save video clips to the PC and/or to portable media such as a USB
stick using remote software. For example, if an incident occurs that requires
police intervention video evidence is quickly and easily extracted from the DVR.
In addition to recording at a rate of up to 400 IPS PAL, the HRDPX16 supports
high-end capabilities such as a user-friendly front panel control, mouse
operation, infra red remote control, express search to quickly find video
evidence, an internal DVD-RW and two USB ports for copying evidence to portable
media.
Honeywell’s HMLCD19LX LCD monitor is designed specifically for the security
industry to provide high resolution display of computer signals and/or composite
video. Because they consume less power, generate less heat and last longer than
conventional CRT monitors, LCD monitors are more cost-effective over long term
use.
“We chose BPS due to our very successful working relationship on many
other projects and their professional approach to completing installations on
programme,” said Conor Cannon of Blackbourne.
“We chose Honeywell because of their quality and cost
effective video solutions,” added Clive Kinnear.
The Benefits: This was a trouble-free installation for BPS, a
company with a wealth of expertise and experience in the fire and security
industry. Importantly, it has met the client’s exact requirements and
specifications and was delivered within the agreed timescales.
A successful video monitoring system should provide the following:
- Peace of mind for the tenants.
- 24 hour surveillance of the building and car park.
- Secure environment to live in.
- Products which are fit for purpose.
Honeywell and BPS were able to deliver on all of the critical success
factors.
Honeywell has a wide portfolio of video products and provides solutions for
many applications.
The choice of cameras was particularly important. Car parks are prone to
cold, damp conditions but are also at risk from vandalism. This made the HD4
vandal resistant domes a perfect choice for this application.
The relatively new HRDP DVR range has proved to be ideal for Obel delivering
straightforward installation and simplicity of operation and providing the
facilities team with a 24 hour video monitoring solution which in turn delivers
peace of mind and security for Obel residents.
“The solution provided for Obel is of the quality we have come to
expect from BPS and Honeywell and will meet our requirements for years to come,”
added Conor Cannon.
Partner of Choice Building Protection Systems NI Ltd BPS has been
a provider of Fire Alarm Systems since 1981 and Security Systems since 1999. The
company has provided design, installation & maintenance of major contracts
to a wide range of clients in Health, Commercial & Retail environments. We
employ in excess of 30 highly trained installation & service team with a
response time of 4 hours to anywhere in Northern Ireland. A locally owned
company, which can resource like a national company, but provides local, quality
assured, 1st class service to customers.
BPS has worked closely with Honeywell Security Group for over 10
years and is an Elite Member of the Honeywell Systems Integrator programme. www.bpsni.co.uk
Blackbourne Integrated M&E Blackbourne Integrated
M&E is an established electrical and mechanical contractor with over 50
years experience in the construction industry sector. It has four main service
divisions; direct works electrical, direct works mechanical, measured term
contracts and facilities management.
Blackbourne is currently working on a number of high profile
projects in each sector. Some of these include Royal Victoria Hospital Critical
Care Unit, Royal Commonwealth Swimming Pool in Edinburgh and Obel at Donegal
Quay Belfast. www.blackbourne.co.uk
Products:
- HRDPX16 - 16 Channel 1Tb Performance DVRs
- HD3VC4SHRX Series Mini Domes
- HD3VC4SHRX Series Mini Domes
- HMLCD17LX 17" LCD Monitors
Honeywell and BPS deliver video monitoring solution to Ireland’s
tallest building – Obel, Belfast (pdf) |