Intrusion Detection System |
 |
Description and Purpose
Intrusion Detection systems sense a number of events that indicate
unauthorized entry into a facility during times when no one should be
present.
In today’s facility, it is typical to include
door/window position sensors,
motion detectors,
glassbreak detection, and
panic buttons.

Figure 1: Typical Intrusion
Detection System
Solving Intrusion Issues
There are a number of critical
issues that are solved with an intrusion detection system.
Unauthorized entry through
doors: Intruders can open a door in many ways, including using prying
tools, torches, or even an issued key to the lock. No matter how the door
is opened, the
door position sensor detects the opening and reports its status to the
control panel for processing.
Protecting Glass Windows:
Entry by breaking glass windows is a common method of unauthorized entry
into a facility.
Glassbreak detectors sense the sound of breaking glass, and then
activate the alarm condition while the intruder is still outside, often
thwarting the attempt. Finding glass break detectors that successfully
sense glass breakage from different types of glass like Tempered,
Laminated, Coated, Wired, Plate, and others is no longer a challenge.
Honeywell offers the most effective glass break sensor for all types of
glass.
Unauthorized entry through
walls and roofs: Some unauthorized entries are achieved by cutting
through walls and facility roofs.
Motion detectors sense movement within protected rooms and departments
of the building. While the Intrusion Detection System is armed, an
activated motion detector causes a local alarm and sends a message to a central
monitoring station.
Crisis during work hours:
When intruders arrive during business hours, employees are often inhibited
from using the telephone to call authorities. A
panic button allows for a discrete, undetected method of calling for
help. You can locate a panic button below counters and desktops to provide
users with an easy, yet subtle method of notifying the authorities. You
can be very specific as to who shall respond to a panic situation, and you
can have many panic buttons for many purposes. See the
Panic Alarm application for more information.
Where to use Intrusion
Detection Systems
There are many facility types
that include intrusion detection systems in the building systems. Some
examples of these facilities include cash
payment centers,
banks,
retail stores,
laboratories,
pharmacies, and
public processing centers.
Intrusion detection sensors are
also used in
energy management applications.
|