|
Creating the best system for your
needs is easy when you use Honeywell’s approach. Generally speaking, for the
most effective system, you need to consider a number of variables that affect
visible scenes, image quality and available storage. You need to be able to
record the right images at a quality level that provides sufficient evidence of
the incident. When cameras work together as a team you can identify specific
individuals, places where they have left fingerprints, actions they performed,
all within the date and time-stamped period which they were present.
Here are some suggestions that raise
the effectiveness of your video system.
-
When designing a
system, there are two main sections that need to be evaluated:
-
Choosing the right
cameras based on what conditions are at each location
-
Choosing the right
head-end based on who will be using the system, how easy it needs to be, how
available it needs to be, what its main purposes are, etc. Different designers
may come up with very different ideas to address these two parts of the system
and so it is very important to listen closely to the needs of the end-users.
-
When choosing a
camera, one of the first decisions is between fixed and PTZ (Pan, Tilt and Zoom)
cameras.
-
Fixed cameras record
one area of view continuously. PTZ cameras can record multiple views, but must
be controlled either by on-site security, surveillance staff or automatically by
using pre-sets or triggers from other systems such as intrusion or access
control. Fixed cameras are less expensive but it will require more of them to
get the same coverage area as a single PTZ. When staff is available, the
advantage of a PTZ is to gain overlapping coverage, with giving up the recorded
views of the fixed cameras.
-
By integrating the
intrusion detection system with the camera system, opening doors and windows, or
triggering a motion detector can cause the video camera to direct itself to the
area requiring observation. The intrusion detection system can apply different
behaviors for when the system is armed, as opposed to when it is disarmed. PTZ
‘s have the ability to take alarm inputs such as a window contact, motion sensor
or glass break, When these inputs are activated, cameras can either go to a
preset position or a tour, which means the camera will pan across an area that
has been previously programmed.
-
Color vs.
Monochrome. Cameras have a wide variety of options which allow the right
camera to be chosen for each location. Color cameras are typically the standard,
unless the area of coverage has inadequate lighting conditions. Today’s color
cameras have much better low-lux ratings than in the past, but monochrome
cameras still have lower ratings. If the area to be viewed has very low
illumination, it still may be best to use a quality black and white camera for
particular areas.
-
Day-Night. The
best of both worlds is to use a day-night camera, or a camera that switches from
color to monochrome when the lux level reaches a certain level. There are two
types of day-night cameras:
-
True Day-Night (TDN).
This camera has a mechanical cut-filter, which is removed when the lighting
conditions drop to a certain level, thus, allowing the camera to operate in
monochrome, which has greater lighting sensitivities and will see more in dark
conditions.
-
Software enhanced
Day-Night (SDN). This camera does the same thing as the true day-night, but via
software instead of hardware. The difference is a slight loss of picture quality
and potential difficulty in adjusting when there is infra-red lighting
NOTE: It is
important to understand that unless a TDN lens is used with a TDN camera; all
the benefits of the camera will not be utilized. A TDN lens, however, should not
be used with a software-enhanced SDN camera.
-
Standard vs. High
Resolution. Cameras typically have a choice between standard and high
resolution. Total vertical lines (TVL) will determine the picture sharpness. The
higher the resolution, the crisper the picture quality, with less graininess.
Higher resolution does carry a higher cost, and some customers may not see
enough difference to pay the higher cost. Also, it is important to note that the
resolution of the camera is only as good as the monitor it will be viewed at, or
the recording device being used. If the monitor is only rated for standard
resolution, a higher resolution camera will bring no value, thus wasting the
additional cost. Also, if the recording device cannot record at the higher
resolution there is no need to use a higher resolution camera.
-
Use cameras at each
entrance to a protected area and at each high-security area like cash registers,
ATMs, and Vending areas. At all key points, it is best to use a grouping of
fixed cameras that ensure you don’t miss any important scenes, and all necessary
areas are covered. Consider the following items you will want to capture at
these key points:
-
Close up of face or
profile
-
Color of clothing
-
Height of individual
-
Build of individual
-
Wide Dynamic Range
(WDR). Lighting conditions at entrances (doorways, lobbies, etc.) can be
very harsh. With the contrast between bright sunlight and the darker interior,
many cameras will not be able to record the necessary detail. In these cases, it
is good to look at Wide Dynamic Cameras which are specifically designed
for areas of extreme lighting contrast. These cameras are more expensive than
standard fixed cameras, but are only necessary in those few entrance locations
and do make a dramatic difference in the quality of video that is recorded.
-
The quality of the
camera will tremendously affect DVR performance. Graininess, low DB levels,
signal to noise ratios, poor video connections – all adversely affect hard-drive
storage, which could easily drive up the cost of a project. Two technologies to
consider combating these issues are DNR and DSS. Digital Noise
Reduction (DNR) removes noise artifacts, improving the performance of motion
detection and typically giving end users the ability to record for longer
periods using their existing DVR unit. Digital Slow Shutter (DSS)
technology improves the light sensitivity of the camera and extends its usable
range.
-
Use cameras at each
transaction location. Consider the following items that you will want to capture
using close-range cameras at nearby locations and long-range cameras when the
camera is located away from the close-up action:
-
Direct activity in
the cash drawer
-
Direct activity of
merchandise being purchased and bagged
-
Images of the
employee and the customer
-
Direct activity at
product counting tables, such as in pharmacies, manufacturing, and other places
where procedures must be monitored.
-
Once each individual
have been identified by entry cameras, you can obtain useful video of general
travel through the building or protected area. Use cameras to collect general
activity views like:
-
General location of
individual in the building
-
An individual’s
general contact with door frames, counters, and things they handle
-
Use clothing colors
and patterns to aid in identifying individuals.
-
If you have multiple
DVRs in a location or organization, it is good to have an overall video
management system to limit confusion.
|