Watching over the Cash Counter

Cash counters can be located in cashier cages, accounting offices, and even next to the cash register. Cash counting activities present risks that can be difficult to manage. When used with proper procedures, video surveillance can offer an effective way to clearly view the counting and handing of cash within the environment. 

Typical uses are shown in the table below. If you are using this document on line, choose applications in the table below to see more information

Protection Options:
Close-up View Validate activity at the cash counter by using a close-up, high resolution view.
General Views View general activity around the cash counter.
Cash Register/Drawer Close-up view of cash being deposited or withdrawn from the cash drawer. Record register transaction information.
Doorways Identify individuals as they enter and leave a room.

 

 

Other Information:
Minimizing System Costs Review a strategy for keeping the cost of the system under control.
Maximizing Video Effectiveness Explore ways to increase the effectiveness of the system.
Control other Costs Determine if the video system can help the user to control other operational costs related to the facility.