Emergency Doors |
 |
Description and Purpose
In
warehouses,
banks,
auditoriums,
restaurants, and
other
facilities, fire door exits must be configured for free exit while
barring entry of unauthorized people. While the door is designed for this
purpose, this type of door can often become the escape route for a thief,
or the unwelcome entry point for non-paying customers.
The system can integrate Emergency Fire
Exits into a more centrally monitored and controlled system, and view
alarms and status of the system from the system
keypad.
Emergency Fire Exits can integrate with the
fire alarm,
intrusion,
remote control, or
panic system so in the event of a crisis, the system can sound a
local alarm at doors to notify staff members of an unauthorized exit. In
addition, the system can integrate
door position sensors to verify the locked status of the door while
closed. The maximum number of emergency doors on the system depends on
the
control panel you choose. |

Figure 1: Emergency Door Exits |
Connections and Considerations
The table below refers to the drawing in
Figure 1. If you are using
this document on line, click the model number in the table below to see
more information.
|
Item |
Model No. |
Description |
Mounting Options |
Notes |
|
D |
4101SN |
Relay: Addressable with zone input |
|
I/O Module |
|
Cs |
4939SN |
Contact: Surface Mount |
Exposed on Door or window Frame |
1.25” gap |
|
O12 |
AD25624 |
Power Supply (DC Voltage indicated) |
In enclosure
(#1451-24) |
Selectable 12VDC or 24VDC operation when using
XF30 transformer. |
|
V |
V-Plex |
V-Plex™ Data Bus |
|
Connects to addressable devices, zone input devices and
relay modules. |
|
Y |
Genesis:
4506 |
2-wire, 18 AWG, Fire rated, Non-shielded |
Use Genesis 1118 for Non-Fire Applications |
This part number is an example. See your building and
electrical codes for actual jacketing requirements. |
Solving Emergency Door Issues
Typical emergency door hardware is an
expensive stand-alone product that usually operates on a small battery for
power. The system can integrate emergency doors using equipment that is
controlled by the main system. When integrating with the system, the
system powers the door hardware, so the user will never need to replace a
9V battery at the door hardware.
When a typical emergency fire exit sounds,
staff members are more likely to search for the reset key than to observe
and report the direction of its unauthorized user. When integrating the
emergency exit with the system, the user will be able to reset and silence
the door from the familiar system
keypad or other user interfaces. Users will not need to search for a
seldom-used reset key.
|