|
When
selecting which system fits your application, consider the number of users that
will be enrolled into the system, how quickly users must be enrolled into the
system, and the kind of users that will occupy the building.
The number of users may not be
the only requirement to consider. Consider the user enrollment requirements for
a campus environment. During class enrollment, there may be hundreds of people
to process during a short time period. This may require multiple enrollment stations and ID badge printing.
Classifying Groups of Users
Similar people access buildings
in similar ways. For example, a group of people who work in the manufacturing
side of the building have different access requirements than a group of people
who work in the administration section of the building. The system can classify
each of these groups to operate the system in similar ways. Classified groups
of people share what may be called Access Levels, Authority Levels, User Groups, or User Profiles.
In the table below, choose a system
to see more about equipment requirements and suggestions suitable for the
application.
System Type
|
Maximum Number of Users per Control Panel
|
Maximum Number of Access Levels
|
|
NetAXS
|
10,000 |
128 |
|
WIN-PAK
SE |
25,000+ |
150,000 (1 or 6 per user) |
|
WIN-PAK PE |
10,000 |
Unlimited with Host
Grant feature |
|
NStar |
10,000 |
10,000 (1 per user) |
|