Supervisor First

Most facilities require Supervisors to be on site before allowing employees into the building. In addition, because the system can unlock selected doors according to a schedule, it is possible for visitors to enter the building before employees arrive.

Examples of conditions that cause supervisors to be late are:

  • Weather conditions
  • Traffic and commuting conditions
  • Sickness and health conditions
  • Other emergencies

If your application requires a higher level of security so that employees are not allowed to enter before a supervisor is present, consider the following items when planning your system:

  • Disallow entry until the security system is disarmed
  • Allow only supervisors to disarm the security system

  • Allow doors to hold open on a schedule only if the security system is disarmed

In the table below, choose a system to see more about equipment requirements and suggestions suitable for the application.

Item
Supervisor First Operation
NetAXS Yes
WIN-PAK SE Yes
WIN-PAK PE Yes
NStar Yes