Honeywell Security

CONTACT & SUPPORT  |  WORLDWIDE  Worldwide Locations    

 Search
Press Releases
  Back
Feb 29, 2016
Honeywell Expands Security Alarm Communications Coverage With Verizon’s Wireless Network

Honeywell today introduced the first in a series of alarm communications radios compatible with Verizon’s wireless network, giving security dealers more options to expand their businesses in alternative cellular coverage areas.

MELVILLE, N.Y., February 29, 2016 - Honeywell (NYSE:HON) today introduced the first in a series of alarm communications radios compatible with Verizon’s wireless network, giving security dealers more options to expand their businesses in alternative cellular coverage areas. The new CDMA-X Radio with Verizon 1XRTT technology supports Honeywell Total Connect Remote Services® and alarm signal transport for fire, burglary and status messages. It comes pre-activated and is remotely upgradable, allowing for a faster installation and lower maintenance costs.
The new line of radios from Honeywell will leverage Verizon’s wireless network, which is based on Code Division Multiple Access (CDMA) technology. Radios registered via AlarmNet Direct can be activated in all Verizon and Verizon partner coverage areas, helping dealers increase their wireless footprint and speed up installations.

senior communications product manager-Honeywell. “Adding the CDMA-X radio to our line of GSM communicators offers a competitive advantage in today’s marketplace—giving dealers more choices, providing more coverage and helping them reach more consumers.” The CDMA-X radio is compatible with Honeywell VISTA® control panels and provides security dealers with an opportunity to earn additional recurring monthly revenue (RMR) with Honeywell Total Connect. For more information, please visit www.honeywell.com/security.


Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. For more news and information on Honeywell, please visit www.honeywellnow.com.

Contact:
Media Contact:Katie Hunt
Honeywell
(763) 954-5379
Katie.Hunt@Honeywell.com



  Back Back to top