Honeywell Security

CONTACT & SUPPORT  |  WORLDWIDE  Worldwide Locations    

 Search
Press Releases
  Back
Jul 15, 2014
Honeywell Adds Compact Surveillance Radar Technology to Vindicator Portfolio

SpotterRF’s Compact, Easy-to-Install Radars Provide More Options to Monitor Expansive Areas at Critical Infrastructure Sites

LOUISVILLE, Ky., July 15, 2014 – Honeywell (NYSE: HON) today announced new radar capabilities for its line of Vindicator security systems used to protect high-profile locations such as large commercial properties, government facilities and military installations.

Honeywell’s Vindicator customers will have access to SpotterRF’s series of Compact Surveillance Radar systems, which can be used to detect intruders along perimeters when traditional ground surveillance radar systems are not practical. The devices – which weigh less than four pounds, use standard Ethernet cables and feature built-in Web servers – are highly effective in monitoring wide areas. For example, these radars are currently used to protect infrastructure such bridges, dams, oil fields and even wildlife.

“Vindicator users need the highest level of security, and SpotterRF’s compact surveillance radar technology meets that goal with its ability to monitor expansive areas,” said Brian Holmes, director of Government Sales and Special Programs at Honeywell Vindicator. “These systems are proven to be effective in homeland security-type applications, which makes them a perfect fit with the Vindicator portfolio.”

“Our channels of distribution are expanding rapidly,” states Logan Harris, CEO for SpotterRF. “Ease of installation, industry standard integration, powerful functionality and our aggressive pricing model make SpotterRF radar a great fit in areas not previously open to radar.”

Nearly 1,000 SpotterRF compact surveillance radars have been deployed across the world. SpotterRF radar is a 2013 recipient of Government Security News’ Border Security Award. Popular Science named its advanced low-cost radar “Best of What’s New.

Honeywell’s Vindicator group has more than 30 years of experience providing high-end perimeter intrusion detection systems. Combining Vindicator’s highly secure Command and Control platform with SpotterRF is an ideal solution for securing perimeters at critical infrastructure sites such as power generation, chemical and oil and gas facilities. Vindicator’s integration to Honeywell’s Pro-Watch® access control and MAXPRO® Video Management System allows customers to have an end-to-end security solution from a single manufacturer.

For more information, please visit: http://www.honeywellvindicator.com


About Honeywell
Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.

Contact:
Ralph Maniscalco
Honeywell
516-577-2803
ralph.maniscalco@honeywell.com



  Back Back to top