<< Back

Press Releases

 
 

Honeywell introduces new Hi-Performance Low Voltage Plenum Wire

PLEASANT PRAIRIE, WI, July 21, 2005 -- Honeywell (NYSE: HON), an industry leading thermostat manufacturer, today introduced a full line of UL Listed PVC and Plenum low voltage wires designed for optimum performance of thermostat controls, doorbells, and heating and air conditioning equipment.

The wire is recommended for use with Honeywell digital and non-digital thermostats to ensure the best possible climate control system performance.

Available in convenient 250- or 500-foot spools, Speedbags™ and pull boxes, Honeywell thermostat wire features polypropylene insulation resulting in exceptional dielectric protection. It strips easily and cleanly for faster installations with reduced jobsite waste, plus has sequential footage markings to let the installer know how much cable is left in a box or on a spool.

Wire construction consists of between 2-12 color-coded, solid copper conductors (AWG 18-20) in a flexible, lightweight jacket that is sunlight resistant. PVC general-purpose wires are offered in white or brown jackets, with the Plenum cables are available in a natural jacket color.

For more information, call (800) 222-0060, or visit www.honeywellcable.com.


Honeywell International is a $26 billion diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; specialty chemicals; fibers; and electronic and advanced materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, Chicago and Pacific Stock Exchanges. It is one of the 30 stocks that make up the Dow Jones Industrial Average and is also a component of the Standard & Poor's 500 Index. For additional information, please visit www.honeywell.com.



This release contains forward-looking statements as defined in Section 21E of the Securities Exchange Act of 1934, including statements about future business operations, financial performance and market conditions. Such forward-looking statements involve risks and uncertainties inherent in business forecasts as further described in our filings under the Securities Exchange Act.


 
Contact:
 
Dan O’Connell
O’Connell Communications, Inc.
708-482-0212
dan@oconnellpr.com

 
Ralph Maniscalco
Honeywell Security & Custom Electronics
516-577-2803
ralph.maniscalco@honeywell.com



 

 Back to top


Search