CONTACT & SUPPORT  |  WORLDWIDE  Worldwide Locations    

Press Releases
Oct 21, 2010
Honeywell Releases Total Connect App for Android™ Smartphones

Service Allows Consumers to Control Security Systems and View Live Video Using Increasingly Popular Mobile Device

MELVILLE, N.Y., Oct. 21, 2010 – Honeywell (NYSE: HON) today released a new Android compatible app for its popular Total Connect services. This app provides lifestyle-enhancing Total Connect features to the growing number of Android users—letting them view streaming video of their homes and businesses on their smartphones as well as control their security systems from any location.

Total Connect is Honeywell’s award-winning service that gives consumers access to their Honeywell security systems or Total Connect video systems from anywhere, anytime. Using PCs, laptops, mobile phones and smartphones, Total Connect customers can arm and disarm their systems, receive e-mail alerts when an alarm trips, and access video from inside and around the premises. In addition to Android, Honeywell provides Total Connect apps for the iPhone® and BlackBerry®. The new Android app is available for free download at Android Market.

“Smartphones are the new norm for staying connected to just about everything – friends, family, work, and everything else in between,” said Gordon Hope, general manager of Honeywell’s AlarmNet business. “Security is an essential part of our lives, so it only makes sense to use these increasingly popular devices to stay connected to our security systems as well.”

When using Total Connect apps, users can toggle between two modes: keypad functions and video viewing. In video viewing, users view live video, record and store video clips, take snapshots and can have custom video clips or pictures e-mailed to them when an event happens, such as when a child returns home from school. The Total Connect for Android app allows consumers to view up to six different cameras from their phones individually.

In the system mode, the app replicates a physical keypad and allows the user to arm and disarm their system, bypass zones and control lights and garage doors. When combined with anti-theft and environmental sensors, end users can receive alerts if valuable objects are moved, and if floods or extreme temperature changes have been detected.

For more information about Total Connect Remote Services, please visit

Honeywell International ( is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit

This release contains "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of fact, that address activities, events or developments that we or our management intend, expect, project, believe or anticipate will or may occur in the future are forward-looking statements. Forward-looking statements are based on management's assumptions and assessments in light of past experience and trends, current conditions, expected future developments and other relevant factors. They are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by our forward-looking statements. Our forward-looking statements are also subject to risks and uncertainties, which can affect our performance in both the near- and long-term. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.

Ralph Maniscalco

  Back Back to top