<< Back

Press Releases

 
 

Honeywell Adds Hi-def Indoor/Outdoor Mini-dome to IP Camera Portfolio

HD4MDIP Provides High-Quality Images with Low Bandwidth Requirements

LOUISVILLE, Ky., July 7, 2010 – Honeywell (NYSE:HON) today released a rugged, indoor/outdoor mini-dome IP camera that provides three times the image resolution of standard analog cameras, yet with similar network bandwidth requirements. The HD4MDIP is the latest addition to Honeywell’s line of high-definition, IP cameras that provide high-quality images to help operators complete investigations faster while reducing the infrastructure needed to support the overall surveillance system.

The true day/night, vandal-resistant, fixed mini-dome provides 720p resolution at full frame rate. It also helps save money with its low power-consumption rate and ability to be retrofitted on many existing digital and network video recorder installations without requiring additional storage capabilities. This dramatically decreases the cost of infrastructure and total cost of ownership.

“When it comes to video surveillance, the top two things on end users’ minds today are picture quality and cost,” said Roberto Testani, product manager, Honeywell Security Group. “HD4MDIP is another example of how Honeywell continues to deliver on the promise of IP by addressing both of those concerns. It provides extremely crisp images at minimal bandwidth, reducing the number of hardware servers needed to manage the system.”

Like the indoor-version HD3MDIP, which Honeywell released earlier this year, the HD4MDIP features an externally accessible web-based menu that lets operators view and control cameras from virtually anywhere. It also features built-in motion detection capabilities and camera tamper detection features that notify users when the camera’s field-of-view is altered, obstructed or blurred. The HD4MDIP also decreases installation and training costs through its simplified set up, which includes the same programming requirements as interior cameras. Because of this, operators can cover a wider range of applications without having to learn new products.

In addition to the HD4MDIP and HD3MDIP cameras, Honeywell’s growing line of IP video technology includes a complete selection of recording solutions and the MAXPRO® VMS video management platform. The company will soon expand its camera line to include a bullet camera and box camera options.

To see how Honeywell’s growing line of IP video solutions can help organizations transition from analog-based video to digital systems, please visit www.honeywellvideo.com or www.thesecuritychannel.com.


Honeywell International (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.


This release contains "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of fact, that address activities, events or developments that we or our management intend, expect, project, believe or anticipate will or may occur in the future are forward-looking statements. Forward-looking statements are based on management's assumptions and assessments in light of past experience and trends, current conditions, expected future developments and other relevant factors. They are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by our forward-looking statements. Our forward-looking statements are also subject to risks and uncertainties, which can affect our performance in both the near- and long-term. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.


 
Contact:
 
Wilma Griffith
Honeywell
502-297-5737
wilma.griffith@honeywell.com

 
Andy Ybarra
Weber Shandwick
952-346-6314
aybarra@webershandwick.com



 

 Back to top


Search