<< Back

Press Releases

 
 

Honeywell Releases Enhanced LYNXR-I Wireless Control Panel

Designed with the Future in Mind, Delivers Enhanced Support to Honeywell Family of Communicators

MELVILLE, N.Y., April 2, 2008 – Honeywell (NYSE: HON) today released an enhanced version of the LYNXR-I Wireless Control Panel. The latest addition to Honeywell’s popular LYNX quick-install family of controls, the sophisticated new LYNXR-I is a combination wireless control, keypad and siren that has been enhanced to support the Honeywell family of GSM/Internet communicators, including the 7845i and 7845GSM.

When used with Honeywell’s Total Connect remote services, LYNXR-I lets customers control their security systems, receive important alerts and stay connected to their homes and businesses from any remote location via the Internet, cell phones, PDAs or any web-enabled device. It’s also an excellent opportunity for dealers to increase recurring monthly revenue (RMR).

LYNXR-1 features include compatibility with all 5800 Series devices and built-in two-way voice, which adds another opportunity for RMR by letting central station operators communicate with homeowners in the event of an emergency. Other key features include voice prompts, a built-in message center, reminders, “Follow Me” and scheduling.

LYNXR-I is highly flexible and can be mounted on walls or placed on tabletops. The quick-install device contains voice prompts to walk dealers through the installation process—reducing time and training costs. Additionally, installing a GSM radio or Internet communicator is easier with the GSML and 7847i-L modules, which install inside the same plastic case as the LYNXR-I with no additional enclosures to mount.

For more information, please call 1-800-467-5875.


Honeywell International is a $36 billion diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London and Chicago Stock Exchanges. For additional information, please visit www.honeywell.com.


This release contains forward-looking statements as defined in Section 21E of the Securities Exchange Act of 1934, including statements about future business operations, financial performance and market conditions. Such forward-looking statements involve risks and uncertainties inherent in business forecasts as further described in our filings under the Securities Exchange Act.


 
Contact:
 
Marni Ogrodnik
Honeywell
516-577-2804
marni.ogrodnik@honeywell.com



 

 Back to top


Search