<< Back

Press Releases

 
 

Honeywell Releases 5805-6 Six Button Wireless Remote Control

New Two-Button Panic Designed to Help Reduce False Alarms

MELVILLE, N.Y., January 15, 2008 – Honeywell (NYSE:HON) today announced the release of the 5805-6 Six Button Wireless Remote Control. Its sleek design—featuring concave keys for a more tactile feel and a two-button panic—helps prevent false alarms. An LED provides the homeowner with information on transmission status and battery condition.

The compact, lightweight design allows the remote to travel with the homeowner, easily fitting onto any keychain or in their pocket. The 5805-6 can also help dealers increase their upsell and closing opportunities and add value to every sale by offering convenient, single-button control of lighting and garage doors with up to eight functions.

The 5805-6 is the newest addition to Honeywell’s popular line of 5800 Series of wireless remote controls, including the 5804-2 two button key, 5804 four button key, 5802MN/MN2 panic pendants and 5804BDV bi-directional remote with voice annunciation.


Honeywell International is a $34 billion diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London and Chicago Stock Exchanges. It is one of the 30 stocks that make up the Dow Jones Industrial Average and is also a component of the Standard & Poor's 500 Index. For additional information, please visit www.honeywell.com.


This release contains forward-looking statements as defined in Section 21E of the Securities Exchange Act of 1934, including statements about future business operations, financial performance and market conditions. Such forward-looking statements involve risks and uncertainties inherent in business forecasts as further described in our filings under the Securities Exchange Act.


 
Contact:
 
Marni Ogrodnik
516-577-2804
marni.ogrodnik@honeywell.com



 

 Back to top


Search