<< Back

Press Releases

 
 

Honeywell Reaches Security Communications Technology Milestone

Delivers 500,000th GSM Alarm Radio; Helping Customers Shift to Digital Alarm Transmission

MELVILLE, N.Y., March 30, 2009 – Honeywell (NYSE:HON) has delivered its 500,000th Global System for Mobile Communications (GSM) alarm radio, a key milestone that further signals the rapid adoption of digital communication technology in the security industry.

Since its introduction in 2007, Honeywell’s GSM radio line has gained distinction for its ability to help security dealers easily switch customers from older radios using standard phone lines to the newest technology with Internet-enabled capabilities. Honeywell’s GSM radios use multiple communication paths to ensure alarm transmission and delivery; if one path fails, another is there to transmit the signal to a central monitoring station.

Additionally, Honeywell’s Internet-enabled radio – the 7845i-GSM – is the backbone of the company’s popular Total Connect offering, which allows customers to stay connected to their homes and businesses using any Web-enabled device. For example, Total Connect allows dealers to offer capabilities such as remote alarm system control via text messaging, and services that allow home and business owners to view real-time CCTV video on devices such as laptops and PDAs.

“Alarm transmission is the heart of any security system, but the traditional methods of transmission have shifted over the last few years as standard phone lines have gradually faded away,” said Jim Callahan, chief operating officer at Ackerman Security Systems. Ackerman, an Atlanta-based firm with more than three decades of experience with wireless alarm monitoring, recently purchased and installed the 500,000th Honeywell GSM unit.

“Honeywell’s GSM radio is very well received,” Callahan said. “Customers have been asking for this type of technology because it fits their needs and lifestyles. And the fact that Honeywell reached this milestone so quickly demonstrates that dealers and integrators who embrace digital communication will increase the value of their accounts.”

Honeywell’s GSM radio line was the security industry’s first to offer redundant communication using the Internet, an approach that better protects homes and businesses. The radios can use General Packet Radio Service (GPRS) and the Internet as primary communication paths and are designed to meet the ever-changing needs of the future. Short Messaging Service (SMS), commonly used for text messaging, serves as a backup communication path. This platform enables dealers to expand services and maintain and increase recurring monthly revenue (RMR) streams. Ackerman, for example, estimates today that every one in four sales includes GSM.

“Dealers and integrators who want to sustain and grow their businesses must keep up with the lifestyle and technological changes their customers are making,” said Gordon Hope, general manager of Honeywell’s AlarmNet services. “Honeywell’s GSM technology was designed with that philosophy in mind. It not only meets customer needs today, it allows dealers to evolve to meet needs in the future. It’s a technology that truly helps strengthen dealers’ relationships with their customers.”

For more information, please visit www.honeywell.com/security.


Honeywell International is a $37 billion diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London and Chicago Stock Exchanges. For additional information, please visit www.honeywell.com.


Este comunicado contiene declaraciones prospectivas tal como se definen en la sección 21E de la Ley de Cambio y Bolsa de 1934, incluyendo declaraciones sobre operaciones empresariales futuras, rendimiento financiero y condiciones del mercado. Dichas declaraciones prospectivas comportan riesgos e incertidumbres inherentes a las previsiones empresariales, tal como se describe en nuestra documentación de acuerdo con la Ley de Cambio y Bolsa.



 
Contact:
 
Ralph Maniscalco
Honeywell
516-577-2803
ralph.maniscalco@honeywell.com



 

 Back to top


Search