MELVILLE, N.Y., March 25, 2009 – Honeywell (NYSE: HON) today announced the launch of the new Total Connect Web Design Tool. The unique online resource, available only to Honeywell AlarmNet central stations and dealers, was designed to allow these customers the ability to incorporate their own brands on the Total Connect web application.
The Total Connect Web Design Tool is easy to use and is a powerful image builder—letting dealers offer their customers the Total Connect suite of services while using the tool’s unique features to build brand awareness. The web application pages can be tailored to reflect a dealer’s company image, including their logo and graphic design. Dealers can also create custom headers—including uploadable images—and have the ability to change the text and font for a completely customized look.
For additional information, please contact AlarmNet at 1-800-222-6525.
Careers with Honeywell