<< Back

Press Releases

 
 

Honeywell Introduces First Self-Diagnostic & Self-Healing HDMI Cable

Revolutionary New Honeywell CURxE Light™ Technology Automatically Corrects A/V Signals for Corrupted HDCP and EDID Data

PLEASANT PRAIRIE, WI, August 29, 2007 –Honeywell (NYSE: HON) today announced the world’s first HDMI digital cable with CURxE Light™ technology that automatically corrects corrupted HDCP and EDID data that would otherwise degrade high-definition picture and multi-channel audio performance.

Honeywell developed exclusive CURxE Light™ technology along with Spectrum Electronics’ Jeff Bocaccio, one of the CE industry’s most respected authorities on HDMI.

“We’ve made this cable intelligent by integrating a chip into the connector that performs two major functions,” said David Coleman, Program Manager, CE Cable Products, Honeywell. “First, the chip’s line driver ‘cures’ corrupted HDCP and EDID data that can lead to serious audio and video artifacts. Second, we added ‘light’ in the form of LEDs embedded into the connector that let installers monitor the most critical elements of the HDMI interface for problems.”

“We are encouraged to see companies like Honeywell develop innovative HDMI products for the marketplace," said Les Chard, President, HDMI Licensing, LLC. "As HDMI proliferates and becomes the de facto standard for connecting home theater and PC devices, companies like Honeywell are leading the way with new applications of the technology to meet specific market needs.

AUTOMATIC SIGNAL CORRECTION
" HDCP and EDID data becomes corrupted as a result of inconsistencies of hardware manufacturers’ implementation of HDMI, or excess transmission distances. Working in the background, CURxE Light Technology automatically cleans the bad data to its intended dynamic range for the best picture quality. Left uncorrected this corrupt data causes dropout of the picture or audio signal, incorrect resolution, intermittent “snow” in the picture, or a pink or blue hued screen.

BUILT-IN DIAGNOSTICS
Four LEDs integrated into the cable’s HDMI connector serve as self-diagnostic monitoring indicators. The four LEDs verify: Hot Plug detection, +5 Volts status, HDCP and EDID, pointing to either downstream, upstream or device problems depending on which LED fails to light. The fix may be as simple as switching inputs on the TV or can require a firmware upgrade of the DVD player, set-top box, AV receiver or other source. This first of its kind diagnostics should help installers save hours of time troubleshooting.

SUPERIOR CONSTRUCTION
To help ensure pure, crystal-clear digital audio and video signals, the new cables feature full-balanced line transition-minimized differential signaling (TMDS); 100% foil shield with 25% overlapping, combined with a 90% tinned copper braid shield; plus bandwidth-maximizing silver-plated copper conductors. The male-to-male cables are designed for HDTV 480i, 480p, 720p, 1080i and 1080p. Lengths range from .5 meters (1.6 feet) up to 15-meters (49.2 feet)

For more information, call (800) 222-0060, or visit www.honeywellcable.com


Honeywell International is a $34 billion diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London and Chicago Stock Exchanges. It is one of the 30 stocks that make up the Dow Jones Industrial Average and is also a component of the Standard & Poor's 500 Index. For additional information, please visit www.honeywell.com.


This release contains forward-looking statements as defined in Section 21E of the Securities Exchange Act of 1934, including statements about future business operations, financial performance and market conditions. Such forward-looking statements involve risks and uncertainties inherent in business forecasts as further described in our filings under the Securities Exchange Act.


 
Contact:
 
Dan O’Connell
O’Connell Communications, Inc.
708-482-0212
dan@oconnellpr.com

 
Ralph Maniscalco
Honeywell Security & Communications
516-577-2803
ralph.maniscalco@honeywell.com



 

 Back to top


Search