WOODBRIDGE, On., October 13, 2006 – Honeywell (NYSE: HON) today announced the
launch of WIN-PAK SE with VISTA integration, a single interface that combines
access control and video with intrusion. The software controls and manages
employee or customer access to designated or restricted areas in any business.
It is ideal for areas such as office buildings, employee and delivery doors,
pharmacies, liquor stores, day care facilities, warehouses, restaurants, and
hospitals.
WIN-PAK SE allows users to manage three separate systems through a single
easy-to-use software interface, which not only saves time and money, but also
improves the level of security by eliminating user code sharing. Upon placing an
access card near a reader, only those users who have been granted access by the
building administrator will be admitted into the facility. The same card can
also be used to arm or disarm a security system. If a card is lost or stolen, it
can immediately be removed from the system.
“WIN-PAK SE with VISTA integration is the next generation of the WIN-PAK
platform,” said John Smith, marketing manager for Honeywell Access Systems. “It
combines industry-leading security products into a powerful, comprehensive
security solution for customers.”
Because the WIN-PAK SE with VISTA integration can prevent users from
accessing a building while the system is still armed, it can reduce false
alarms. In addition, alarms associated with intrusion and access control through
the WIN-PAK SE software interface can be quickly retrieved and played back
easily. Automated reporting allows users to send up-to-date reports on intrusion
and access events hourly, daily, weekly, or monthly.
“By combining access control and video with intrusion in a single powerful
interface, we now offer a complete ‘One Honeywell’ solution to our customers,”
said Joe Crowley, product marketing manager, Honeywell Security & Custom
Electronics. “WIN-PAK SE is expandable to meet the current and future needs of
users as their security requirements change.”
Honeywell will demonstrate WIN-PAK SE with VISTA integration at Security
Canada International Security Conference & Exposition 2006. For more
information, contact your local sales representative or visit www.honeywellaccess.com.