<< Back

Press Releases

 
 

Honeywell Adds Enhancements to Touchscreen Keypad Family

6271C Now Features Trilingual Capabilities and New Colour Choices to Enhance Aesthetic Appeal

WOODBRIDGE, ON, Oct. 5, 2009 – Honeywell’s (NYSE:HON) newest enhancements to its line of 6271C Graphic TouchCenter Keypads include trilingual capabilities and a wider choice of colours to complement any interior decor.

Available in silver, black or white, the 6271C is ideal for numerous residential and commercial environments, including kitchens with stainless steel appliances, living rooms with flat-screen TVs and entertainment centers, garages, lobbies, warehouses, offices, industrial settings and more. Three language options—English, French Canadian or Spanish —also aid in creating a more user-friendly touchscreen that that appeals to a wider range of customers. The additions add to the keypad’s simple-to-use design, which guide end-users via menu-driven prompts and icons for intuitive, easy security system control.

“The ability to easily blend into existing home or business surroundings provides a stronger sell for dealers, and incorporating more languages increases the customer base,” said Chris Welling, Vice President, Sales for Honeywell. “Combining these new features with the sharp graphics and intuitive display makes the 6271C an eye-catching device that simplifies security for the end user.”

Compatible with many of Honeywell’s popular control panels, the 6271C keypad offers intuitive operating functions, including lighting and garage door control and voice annunciation of system status and zone information for an added level of protection. The device also offers home-screen customization, allowing dealers to showcase their logos on the large, colour touchscreen display. Additionally, end users can upload personal photos to the display.

For more information, please call 1-800-467-5875.


Honeywell International (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.


This release contains forward-looking statements as defined in Section 21E of the Securities Exchange Act of 1934, including statements about future business operations, financial performance and market conditions. Such forward-looking statements involve risks and uncertainties inherent in business forecasts as further described in our filings under the Securities Exchange Act.


 
Contact:
 
Lori Herder
Honeywell
905-856-2384 Ext. 5104
lori.herder@honeywell.com



 

 Back to top


Search