<< Back

Press Releases

 
 

Honeywell Expands Popular Access Control Family

Web-based NetAXS™ System Now Available in 2-Door Option

BURGESS HILL, UK, June 15, 2009 – Honeywell (NYSE: HON) today introduced a version of its popular NetAXS web-based access control panel ideal for small installations. The new NetAXS™ 2-door web-based control panel provides all the security of an access control system with the convenience of managing it via a web browser. The panel allows users to protect as few as two doors and add more panels as needs change. In addition, the new NetAXS 2-door control panel can be used in conjunction with current NetAXS 4-door panel solutions to meet any access control requirements that customers may have. By combining the 2-door and 4-door solutions over any Ethernet network, users now have a powerful choice that can fit almost any application.

NetAXS is quick and easy to install and offers a cost-effective alternative to traditional PC-based systems because it allows end users to easily customise the level of security and functionality based on their needs. The system’s built-in web server allows end users to manage the system anywhere an Internet connection is available or alternatively by connecting a laptop directly to the panel’s Ethernet port. The web browser allows a customer to run reports, monitor events and alarms, and add and remove users. This flexibility is ideal for remote activity such as facility check-in, managed access and manual override of doors or time zones. With no PC software to install, customers who choose the web interface have no worries about operating system compatibility, virus attacks or other computer issues such as hard drive crashes or system lock-ups.

The NetAXS 2-door control panel can also be added to most installations that use Honeywell’s WIN-PAK® access control system and offers additional benefits over Honeywell’s traditional N-1000 control panels including on-board Ethernet, an expandable footprint, larger memory capacity and faster processing.

“With the addition of this new panel to the NetAXS family, we can offer an access control solution for any size facility,” said René von Franquemont, access control product marketing manager for Honeywell Systems Group EMEA. “This new panel is a strong addition to our access control offering. Its basic functionality provides greater flexibility in cost-effective security system design to answer the needs of our value-driven customers. The installer-friendly features and the intuitive browser-based interface enable NetAXS to be confidently installed by all, including those new to access control.”

For more information, visit www.honeywell.com/security/uk.


Honeywell International (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.



This release contains certain statements that may be deemed “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements.


 
Contact:
 
Sue Howes
Honeywell Systems Group EMEA
00 44 7766 420250
sue.howes@honeywell.com

 
Guy McGerr
Weber Shandwick Technology
00 44 20 7067 0337
gmcgerr@webershandwick.com



 

 Back to top


Search